On the Ref Man I read:
the FORCE_COLD_BOOT should be reflected in SRC_SBMR...
I looked for SRC_SBMR and found two registers, but in neither of them do I seem to see the bit reflected by the FORCE_COLD_BOOT fuse.
Could you point me to which register and which bit I find it in?
best regards
Max
Solved! Go to Solution.
Hi @mastupristi ,
For RT1170, I think this fuse bit is not touched by ROM. You can ignore it.
Regards,
Jing
I think this fuse bit is not touched by ROM. You can ignore it.
Is this your feeling or do you have written confirmation in some document?
Because the only document I have available says the fuse is there and it's reflected somewhere on SRC.
best regards
Then I suggest removing the description of that fuse from both the Refernce Manual and the Security Refernece Manual
best regards
Max