RT1176 transfer data through usart at baudrate 921600

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

RT1176 transfer data through usart at baudrate 921600

跳至解决方案
2,121 次查看
wangfan_1987
Contributor I

Hi:
I have a large mount of data to transfer through usart,so I need a high speed baudrate.But I meet some problem when change the baudrate.

  1. In the baudrate 115200 and 460800,the usart work well,I got the "hello world".
  2. When I try to change the baudrate in BOARD_InitDebugConsole() defined by the macro BOARD_DEBUG_UART_BAUDRATE to 921600,I got a garbled code.

I want to know how much is the top baudrate of the usart?Can I do some changes to make the usart work normally.

0 项奖励
回复
1 解答
1,771 次查看
Padi-2023
Contributor III

1702628466529.png
After reading NXP data for an afternoon, please refer to LPC55S1x/LPC551x User manual "UM11295.pdf", I tried to use 1000000bps, RT1176 development board can work normally.

在原帖中查看解决方案

11 回复数
1,772 次查看
Padi-2023
Contributor III

1702628466529.png
After reading NXP data for an afternoon, please refer to LPC55S1x/LPC551x User manual "UM11295.pdf", I tried to use 1000000bps, RT1176 development board can work normally.

1,662 次查看
wangfan_1987
Contributor I
Since the core frequency of IMXRT1176 is relatively high, configuring it with a baud rate of 921600 should not be a problem. If there are no issues at a baud rate of 1M, then the hardware communication on the circuit board should also be fine. This is a peculiar phenomenon. Nevertheless, thank you for your solution.
0 项奖励
回复
2,061 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @wangfan_1987 

I did the testing myself and it works correclty, I only changed the macro value just like you did.

Can you help me sharing the value of the BAUD register?

You can access it while debugging, on the peripherals.

Miguel04_0-1695849452573.png

 

Best Regards, Miguel.

0 项奖励
回复
2,046 次查看
wangfan_1987
Contributor I

Thanks for your reply!

My Test board is MIMXRT1176-EVK REVA1,used a USB cable connect the board to PC to transfer usart1 data.

My test program is D:\wangfan\NXP\MIMIX1176\SDK_2_12_0_MIMXRT1170-EVK\boards\evkmimxrt1170\rtos_examples\freertos_hello\cm7

when run the program I want to get "48 65 6C 6C 6F 20 77 6F 72 6C 64 2E" ,which mean "hello world",while I get  "62 AC 3B B8 3E AC 3B 09 FF ".But in baudrate 115200,it was right.

The register value as following:

wangfan_1987_0-1695863652274.png

 

0 项奖励
回复
2,033 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @wangfan_1987 

Can you share with me your IDE version? Your SDK version is 2.12, correct?

I'll look into it and let you know what I found.

Best Regards, Miguel.

0 项奖励
回复
2,021 次查看
wangfan_1987
Contributor I

Thanks for your reply! 

My IDE version is KEIL 5.33.0,My compiler is V6.15::ARMCLANG.The SDK pack  name is SDK_2_12_0_MIMXRT1170-EVK.zip,So I think it is the version.I am very thankful for your help!

0 项奖励
回复
1,796 次查看
Padi-2023
Contributor III

hi! I also encountered the same problem, so long you should have solved it! May I ask how it is solved? thanks.

0 项奖励
回复
1,793 次查看
wangfan_1987
Contributor I
Not sloved,just use a lower baudrate.Maybe core clock problem,if I have enough time,I will tyr to slove.:(
0 项奖励
回复
1,791 次查看
Padi-2023
Contributor III
I searched the NXP official website forum and found no solution, I think it is not supported to this piece, 24000000/921600=26.04166666667, 24000000\26=923076.923076, (923076.923076-921600) /921600*100%=0.16%, in fact, the error rate is 0.16%, according to this error rate can be used, even if the interface clock of kCLOCK_Root_Lpuart1 is raised, it may not be solved.
0 项奖励
回复
1,787 次查看
Padi-2023
Contributor III
Why do I think this is not supported by this piece? Since the RT685 I am using here is also set with this baud rate, no problems have been found so far
0 项奖励
回复
1,965 次查看
Miguel04
NXP TechSupport
NXP TechSupport

Hi @wangfan_1987 

Thank you for the information, however you are using an outdated SDK version and another ide.

I'm using MCUXpresso IDE and this is recommended by NXP to use our platforms, I did not face any issue while using this IDE.

Best Regards, Miguel.

0 项奖励
回复