On an RT1051 I use QTIMERS to make PWM signals.
I need that when I set 0 to duty the output stays low, while if I set 100 it stays high.
I have tried by modifying the SDK example by imposing
QTMR_SetupPwm(BOARD_QTMR_BASEADDR, BOARD_QTMR_PWM_CHANNEL, QTMR_PWM_OUTPUT_FREQUENCY, 0, false, QTMR_SOURCE_CLOCK);
or
QTMR_SetupPwm(BOARD_QTMR_BASEADDR, BOARD_QTMR_PWM_CHANNEL, QTMR_PWM_OUTPUT_FREQUENCY, 100, false, QTMR_SOURCE_CLOCK);
but I cannot get the desired result
how can i get what i want?
best regards
Max
解決済! 解決策の投稿を見る。
Hi,
if I understand correctly there is no way to avoid glitches when I set duty 0% or 100%, right?
>>>>Yes, no way to avoid the glitch for the 0% or 100% percent. As a workaround, if you do not want any glitch, in the application code, when the duty cycle is 0% or 100%, you can set the pad as GPIO output mode and output low or high.
BR
XiangJun Rong
Hi,
The 100% percent and 0% percent are extreme examples, if you use the other percent for example from 1% to 99%, is the PWM duty cycle okay?
The QTMR_SetupPwm() uses the variable-Frequency PWM mode, the TMR_COMP1 represents the PWM LOW logic time, the TMR_COMP2 represents the PWM high logic time(dependent on plarity of PWM signal).
The PWM period value is QTMR_SOURCE_CLOCK/QTMR_PWM_OUTPUT_FREQUENCY, the TMR_COMP2 represents the high time, it is (duty cycle percent)*QTMR_SOURCE_CLOCK/QTMR_PWM_OUTPUT_FREQUENCY.
The TMR_COMP1 represents the LOW time, it is (1-duty cycle percent)*QTMR_SOURCE_CLOCK/QTMR_PWM_OUTPUT_FREQUENCY.
For the extreme duty cycle 0% and 100%, one of the TMR_COMP1 or TMR_COMP2 is zero, do you see glitch or whatever?
For detailed information, pls refer to section 46.6.5.14 Variable-Frequency PWM Mode in IMXRT1050RM.pdf
BR
XiangJun Rong
if you use the other percent for example from 1% to 99%, is the PWM duty cycle okay?
Yes
For the extreme duty cycle 0% and 100%, one of the TMR_COMP1 or TMR_COMP2 is zero, do you see glitch or whatever?
Yes
so if I understand correctly there is no way to avoid glitches when I set duty 0% or 100%, right?
best regards
Max
Hi,
if I understand correctly there is no way to avoid glitches when I set duty 0% or 100%, right?
>>>>Yes, no way to avoid the glitch for the 0% or 100% percent. As a workaround, if you do not want any glitch, in the application code, when the duty cycle is 0% or 100%, you can set the pad as GPIO output mode and output low or high.
BR
XiangJun Rong