RT1050

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050

2,038 Views
616602356
Contributor I

我司做一批RT1050的板卡(第一次量产,样品没有问题),有大概率启动失败的问题,具体失败详细情况如下:

1. 抽取20张首次烧录后的RT1051板卡,每张板卡上电10次,其中2张板卡出现上电初始化失败的情况,这两张卡不良的概率为8/10, 7/10;

   再次升级相同固件后,测试,20张RT1051板卡出现5张上电初始化失败(包含首次测试的2张),其失败的概率分别:1/10,2/10,3/10,7/10,8/10;

 

2. 使用之前初始化失败概率在9/10以上的板卡两张,更换同批次的M7主芯片,更换后20次未出现上电初始化失败的情况;(芯片丝印 MIMXRT1051CVL5B IN04V CTAG1813A)

3、每次启动失败时,调试串口输出的LOGO均在卡在

DRAM:34MB

我司使用的RT1051+HYPER Flash+34MB SDRAM。

请帮忙是否可以处理一下此问题?谢谢!!

Labels (1)
0 Kudos
Reply
1 Reply

1,820 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Kang,

   According to your description, the most likely reason for the issue is caused by 'Pseudo Soldering', because after changing RT1051 to be a new one, 20-time booting was successful. 

   So my suggestions are :

   Abstract some samples in mass-produced products , and reheat RT1051 on board by BGA workbench. Then burn image into hyper flash, and check if issues have solved.

----in Chinese---

按照您的描述,虚焊的可能性很大,因为更换了RT1051之后,20次启动都没有问题。

我的建议是:

从量产的产品中抽出一些做样品,在BGA工作台上,重新加热RT1051部分。然后在测试,看是否能解决问题。

目前看,设计是没有什么问题的。

另外,顺便提一下:34MB的SDRAM不太对,应该是32MB才对。你可以把你内存工作的clock打印一下,或 检查一下代码,SDRAM时钟目前是多大。

------------------------

Have a nice day!

TIC Weidong Sun

0 Kudos
Reply