RT1050 Flexio SPI

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 Flexio SPI

1,489件の閲覧回数
christiangradl
Contributor III

Hi, i'm running spi master on flexio.

what is the maximum clock frequency for flexio?

(lpspi has 30 MHz, thats too low for my application)

Thanx

ラベル(1)
0 件の賞賛
返信
1 返信

1,157件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Christian

flexio timings are described insect.27.4.4.2 Pin Synchronization,

sect.27.5 Application Information, sect.27.5.3 SPI Master i.MX RT1050

Processor Reference Manual :
maximum baud rate is divide by 4 of the FlexIO clock frequency.


https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Max. frequency can be found in Table 18-4. System Clock Frequency Values

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信