RT1050 Flexio SPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT1050 Flexio SPI

1,458 Views
christiangradl
Contributor III

Hi, i'm running spi master on flexio.

what is the maximum clock frequency for flexio?

(lpspi has 30 MHz, thats too low for my application)

Thanx

Labels (1)
0 Kudos
Reply
1 Reply

1,126 Views
igorpadykov
NXP Employee
NXP Employee

Hi Christian

flexio timings are described insect.27.4.4.2 Pin Synchronization,

sect.27.5 Application Information, sect.27.5.3 SPI Master i.MX RT1050

Processor Reference Manual :
maximum baud rate is divide by 4 of the FlexIO clock frequency.


https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf

Max. frequency can be found in Table 18-4. System Clock Frequency Values

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply