Hi,
I got doc from FAE, but I want to confirm some step.
Please check.
1. For pdf page 3 "Tools", I got image_enc.exe from FAE and rename to ”image_enc.exe".
2. In page "Project modification", SDK Example: I use evkmimxrt1015_igpio_led_output SDK and generate evkmimxrt1015_igpio_led_output.s19 file with XIP_BOOT_HEADER_ENABLE=0 and XIP_BOOT_HEADER_DCD_ENABLE=0.
3. I prepare a folder and make all utility file in the same path and create a batch file.
4. In page 7 Generate secure image.
I change to
elftosb.exe -f imx -V -c imx-flexspinor-normal-unsigned.bd -o ivt_igpio_led_output_srec.bin evkmimxrt1015_igpio_led_output.s19
5.
My script is "image_enc.exe ifile=ivt_igpio_led_output_srec.bin ofile=ivt_igpio_led_output_srec_encrypt.bin base_addr=0x60000000 region0_key=00112233445566778899aabbccddeeff region0_arg=1,[0x60001000,0x2000,0]"
6.
I made a tool to remove first 1KB data.
My script is "RemoveBinaryBytes.exe ivt_igpio_led_output_srec_encrypt.bin ivt_igpio_led_output_srec_encrypt_remove1K.bin 1024"
My output is ivt_igpio_led_output_srec_encrypt_remove1K.bin.
7.
My script is "elftosb.exe -f kinetis -V -c program_flexspinor_image_hyperflash_encrypt_sw_gp2.bd -o boot_image_encrypt.sb ivt_igpio_led_output_srec_encrypt_remove1K.bin"
The final sb file is "boot_image_encrypt.sb".
I attach all of my script and bin file.
8.
I think the boot_image.sb is the boot_image_encrypt.sb file.
But in this step, I am confused.
From AN12079, I guess it should modify the ucl2.xml file, but my doc doesn't mentioned about it.
Here is the page 29 of AN12079.
Sorry I change to simplified Chinese here.
疑问一:
我的program_flexspinor_image_hyperflash_encrypt_sw_gp2.bd档案当中
section(0)里面的动作,是不是都要透过blhost去执行,我必须跟AN12079一样,加上blhost receive-sb-file的command
FAE给我的doc中,只提到将Flashloader的ini里面的name改成 name = MXRT105X-DevBoot
我认为这边是有问题的
疑问二:
program_flexspinor_image_hyperflash_encrypt_sw_gp2.bd档案当中
sources {
myBinFile = extern (0);
}
以及
#5. Program image
load myBinFile > kAbsAddr_Ivt;
我看不懂是将哪一个档案load到kAbsAddr_Ivt这一个位置?
Assign to Kerry
To Kerry: 你可以使用英文或中文回覆
附件有我的SDK和我的script以及FAE提供的doc
Regards
Ken
楼主你好!
感谢你新建case的合作,已经收到最新回复你关于usb工程重设SP的方法解决了你的问题。
另外,昨天和我们的AE讨论了你的问题并证实给你的方案能解决问题之后,我们热心的AE也写了一篇更深入的文章来讲之前代码跑飞的原因,如果有时间,欢迎查看我们AE的文章:
https://www.cnblogs.com/henjay724/p/13652875.html
一定能让你收获颇丰。
如果还有任何新的问题,欢迎新建case或者新建问题贴!
楼主你好!
我记得你这个帖子后面好像有个测试某个app有问题的情况,现在论坛改变了,我很难直接找到你后续的问题。
所以,你那边是否可以重新建一个case,可以说分配给kerryzhou,这样我可以在新的帖子里面回复你。
现在新的论坛,不太好在很长的帖子里面找你当时的问题,感谢你的理解。
Wish it helps you!
If you still have questions about it, please kindly let me know!
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------
Hi Kerry
不确定你有没有看到我的回覆,如果你有什么建议,请再回覆我
謝謝
Ken
Hi Ken Su,
你那边是否有所更新,是否能照着我的步骤完成命令烧写BEE 并成功Boot?
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry
这边想先跟你确认
RT1015 APP BEE encryption operation method
这边提到app file preparation,我发现你没有提到要手动更改Flash位址设定
因為我拿到的SOP提到
"Modify the memory configuration start from 0x60002000"
这个部分其实是不需要的吗?
Regards
Ken
Hi Ken Su,
如果你查看我的evkmimxrt1015_iled_blinky_0x60002000.s19文件,你会发现我的文件直接就是从0X2000开始的。
其实你不需要手动改,你看我这边是从0x60000000放firmware:
但是,你注意,你看我XIP_BOOT_HEARDER_ENABLE是不是配置为0了?
XIP_BOOT_HEARDER_ENABLE=0,意味着,我生成的.s19文件不带头,不带哪些头呢?
1. 从0x60000000开始放的CFG代码
2. 从0X60001000开始的IVT代码
这些代码,我都交由commander line,或者MCUBootUtility去添加了。
所以你看我就算不改地址,我的app照样是从0X60002000开始存放。
如果你完全按照我的步骤走,你不需要修改你的memory 起始地址。
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry
谢谢解释
我懂了
关键是XIP_BOOT_HEARDER_ENABLE=0
我目前一样使用NXP的RT1015 EVK,这片板子之前做过很多次MCUBootUtility的测试,
如果我使用All-In-One-Action 程式似乎就当掉了,不会动作,只能强制关闭
因此我才会透过"Image Loading Sequence"的Load Encrypted Image
但是我每次操作都会出现以下的错误讯息
因此我直接使用Blhost tool将"ivt_evkmimxrt1015_igpio_led_output_unsigned_bee_encrypted_nocfgblock.bin"这个档案,直接烧到0x60000400的位置 --> 这样是可以的吗?
即使这样,EVK SW8 设定为 1-ON,2-OFF,3-ON,4-OFF重开机后,EVK依然进入Download mode
这边我想确认一下,BEE XIP会需要用到0x680 (SW_GP1[31:0])吗?
因为我发现MCUBootUtility会把它也锁住
附上我的eFuse
我会再继续确认
Regards
Ken
Hi Kerry
上午好
我将你8/17放上去的附件
产生出来的boot_image_encrypt.sb档案,透过MFGTool(我使用1020的)下载到板子上
下载的方式就是使用MXRT102x-DevBoot 的ini设定
LED开始闪烁,因此我认为是Image成功运作
接下来我确认有哪些差异时,我发现我自己编译出来的s19不太一样
后来我发现我的专案用的是evkmimxrt1015_igpio_led_output
再次确认后,我改用一样的专案evkmimxrt1015_iled_blinky ,
我产生出来的s19档案依然和你的不一样,但我烧进去是可以运作的,
我修改source把LED闪烁的频率加快,确认也没有问题
我s19檔案產生的方式是使用
我想这应该是没问题的
毕竟我可以烧进去我自己修改过的evkmimxrt1015_iled_blinky
现在我想唯一的差异是
evkmimxrt1015_igpio_led_output编译出来的s19档案比较大了一点
使用evkmimxrt1015_igpio_led_output
MFGTool烧录就会出现错误
我想是Size不同 应该要修改一些设定
Regards
Ken
Hi Ken Su,
那么总之,你现在那边也能用你自己的代码烧进去工作了,只是有个别的代码不能运行,比如evkmimxrt1015_igpio_led_output直接生成你那边不行,对吧?
我还有个办法,就是修改imx-flexspinor-unsigned.bd
options {
flags = 0x00;
startAddress = 0x60000000;
ivtOffset = 0x1000;
initialLoadSize = 0x2000;
//DCDFilePath = "dcd.bin";
# Note: This is required if the default entrypoint is not the Reset_Handler
# Please set the entryPointAddress to Reset_Handler address
// entryPointAddress = 0x60002000;
}
这里,entryPointAddress, 你把它直接写成你image reset的入口地址,你看下你的app.s19。
比如我的.s19,可以写成
entryPointAddress = 0x600021A9;
你这样试试去生成IVT,然后再跑看看是不是就行了。
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry
我update目前的状态
目前我一共试了以下的SDK范例
除了evkmimxrt1015_dev_cdc_vcom_freertos.s19之外,其余的都可以跑
原先evkmimxrt1015_igpio_led_output.s19无法跑,而且是MFGTool就出错,因此我认为可能Erase空间不足,
我把Erase加大后,就可以跑了,其余的专案也都可以
唯独evkmimxrt1015_dev_cdc_vcom_freertos.s19依然无法
现象是MFGTool烧录成功,但是Image没有跑起来
我有试过entryPointAddress = 0x600022A9; //
结果是无效的
这边有什么建议吗?
Regards
Ken
Hi Ken Su,
这个例程:
evkmimxrt1015_dev_cdc_vcom_freertos.s19
如果你不用加密模式是否能跑?
还有0X60002000偏移入口是否试过?
这个代码应该是比较大的,查看下代码大小,擦除尺寸包含整个image空间。
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry
我确认过无加密的状态下
evkmimxrt1015_dev_cdc_vcom_freertos 是可以成功执行的
Erase部分目前我是加到1MB,应该已经足够了
还有0X60002000偏移入口是否试过?
-->你指的是 加上entryPointAddress = 0x600022A9; 吗 (這邊有試過了)
Regards
Ken
Hi Ken Su,
evkmimxrt1015_dev_cdc_vcom_freertos 无加密可以,BEE加密就不行,是这个意思吗?
用MCUBootUtiltiy烧录也不行?
入口地址entryPointAddress=0x60000000, 还有ResetHandler都试了也是一样情况,对吗?
如果确实是这样,你先测试其他可以工作的,这个等我有空帮你测试下。这几天可能没有时间测试,明后天我休假,今天还有很多case需要测试,所以你先做其他可以用的,这个问题等我抽出空,帮你测试下看看具体i情况。
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry
是的
非常谢谢你的帮忙,等你有空再帮我确认
因为我的案子 就是根据evkmimxrt1015_dev_cdc_vcom_freertos做为base开发的
evkmimxrt1015_dev_cdc_vcom_freertos 无加密可以,BEE加密就不行,是这个意思吗?
-->是的 目前是这样
我會再繼續試
Regards
Ken
Hi Ken Su,
那么你有没有用MCUBootUtilitytool 去在BEE模式下下载这个evkmimxrt1015_dev_cdc_vcom_freertos代码,是否也是不能工作?不过话说回来,如果不加密可以,加密不行,可能还是和BEE的模块哪些限制有关了,具体我还需要时间去深入查看。
不管怎样,你那边测试有任何更新,都请告诉我!
你那边app可以先在非加密模式下去开发,等我后面慢慢去看这个到底和BEE哪些限制有关了。
Wish it helps you!
If you still have questions about it, please kindly let me know.
Best Regards,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Kerry
MCUBootUtilitytool
我一直都有会当掉的问题,下图是使用All-In-One-Action
这边有机会跟Jay确认吗?
Regards
Ken
Hi Ken Su,
你这个问题,我建议你把MCUBootUtility放到比较浅的路径下面,有可能是软件放的路径比较深的原因。
比如你放到桌面路径试试,看看是否能解决这个问题?
如果还有问题,还请告诉我。
Best Regards,
Kerry
Hi Kerry
早安
后来我将MCUBootUtility移到另一台电脑就可以正常执行,但后来还是无法跑evkmimxrt1015_dev_cdc_vcom_freertos这一个SDK范例
昨天我同事发了一个地方,设定XIP_BOOT_HEADER_ENABLE=0,他直接在MCUXpresso上面开始单步执行,发现程式跑到某一行后就当掉了
于是先将这一行注解掉,程式就可以正常跑
接下来我一样用Script加密的方式,将注解掉这行CODE的Image,测试BEE XIP
我发现他也能执行了!
因此XIP_BOOT_HEADER_ENABLE=0
从实验来看,他影响了程式的执行
PS: evkmimxrt1015_dev_cdc_vcom_freertos这个范例我有确认过XIP_BOOT_HEADER_ENABLE=1的设定下是可以跑未加密的模式
你这边有什么看法吗? 这会是Bug吗?
Regards
Ken
Hi Kerry
还有一点想要确认
我将我的EVK设定为SW8 设定为 1-"OFF",2-OFF,3-ON,4-OFF,烧录没有加密的Image,
Image可以正常执行,我这样做是为了确认我的板子跟IC还是正常运作的。
接下来
我做了一个实验SW8 设定为 1-"ON",2-OFF,3-ON,4-OFF,一样烧录没有加密的Image,
Image还是可以正常执行,这是合理的吗?
Regards
Ken
Hi Ken Su
我认为,如果芯片读取前面的 EKIB, EPRDB区域,没有有效数据,然后就认为你是没有加密,并且按照无加密image去执行了,所以这个应该不算有问题。
你现在是使用我的image可以,你自己的image就不行,对吗?
Best Regards,
Kerry