hi,
we have a question regarding the flash NOR RW freq .
we currenty working on a custom board using the RT1176 , we are implementig a flashloader a bootsel and a bootloader as we want to boot from IS25LP128 SERIAL FLASH MEMORY WITH 133MHZ MULTI I/O SPI & QUAD I/O
so the boot flow is perfect when running on 60Mhz serialClkFreq , but we need to raise that to 133Mhz
after Refernce manual lookup , we found that we need a to mux a FLEXSPI DQS pin and change the sampling to readSampleClksrc= kFlexSPIReadSampleClk_LoopbackFromDqsPad .
but when looking for pin mux options we found 3 choices basicaly AD_17 , SD_B2_05 and EMC_B2_18
we tried three of them and none worked (no boot)
is there anything else we're missing !
thank you
Yosri
#i.MX-RT1176
Solved! Go to Solution.
Hi @yosri_c
Not all FlexSPI Pinmux combinations can be used to connect to serial NOR Flash for boot.
About boot pin, please refer to the system boot chapter in the RM manual.
Hope this will help you.
BR
Hang
hi @HangZhang ,
okay thank you for the reply ,
we're just conserned and want to know the use of the PIN GPIO_EMC_B2_18 is it deprecated and doesn't support DQS functionality anymore ?
because we still have it in the refernce manual as a DQS pin .
Thank you so much indeed for clarifying this
Hi @yosri_c
Not all FlexSPI Pinmux combinations can be used to connect to serial NOR Flash for boot.
About boot pin, please refer to the system boot chapter in the RM manual.
Hope this will help you.
BR
Hang
hi ,
i read the section and that's why i asked , the GPIO_EMC_B2_18 pin was used in a previous RM as FlexSPI_DQS_A pin , and then i read about it in another thread that it will be depracated !
my question was , does this pin support the DQS function or not anymore
( RT1176 - flexSPI DQS connection for max R/W speed - NXP Community )
Thank you
Hi @yosri_c
According to the rt1170 RM, it can be used as FLEXSPI1_A_DQS pin.
But for Boot, it can not be used as DQS pin.
Hope this will help you.
BR
Hang
Hi @yosri_c
When the transmission rate is relatively high, in order to transmit data more accurately, DQS is provided by flash.
So you can try to config
config.rxSampleClock = kFLEXSPI_ReadSampleClkExternalInputFromDqsPad.
And config the pin mux that you mentioned.
Hope this will help you.
BR
Hang
hi,
thank you for the answer . as i mentionned we already changed the sampling config to kFLEXSPI_ReadSampleClkExternalInputFromDqsPad.
we changed the .serialClkFreq = kFlexSpiSerialClk_133MHz
we muxed the pin
Hi @yosri_c
Are you using the Primary Pin Group or the Secondary Pin Group?
According the i.MX RT1170 Reference Manual. For the secondary pin group, the Maximum Flash
frequency supported on this port is 100MHz.
.
And have you chosen this frequency?
Hope this will help you.
BR
Hang