Question about DCD version field on RT106x

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Question about DCD version field on RT106x

913 次查看
carstengroen
Senior Contributor II

In the UM for RT1060 it is shown that the Version field of the DCD data must be 0x41:

pastedImage_1.png

However, in the evkmimxrt1060_sdram_ini_dcd.h it is set to 0x40.

pastedImage_2.png

Which one is correct ?

标签 (1)
0 项奖励
回复
2 回复数

785 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Carsten

it can be both as described in Figure 8-15

pastedImage_1.jpg

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

785 次查看
carstengroen
Senior Contributor II

Thanks Igor,

but that is for the IVT, the one I referenced above is the DCD ?

0 项奖励
回复