Parity Backed RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Parity Backed RAM

1,218 次查看
scribble
Contributor I

Hi guys,

The i.MX RT range appears well suited for industrial application and I'm eager to use it in a data logging project, however, my data logging will track accumulated values over a long period of time and so it's important to me that these values remain accurate.

Some competitor products offer parts of RAM that are parity backed to ensure their integrity or at the very least detection of an error. I can't find any mention in the datasheets of the i.MX RT series but just thought I'd ask if parity checking in RAM is supported? As manufacturers don't always think to list this information. If not, this would potentially be a good feature to see in future silicon.

Many thanks

0 项奖励
回复
3 回复数

1,063 次查看
b36401
NXP Employee
NXP Employee

Unfortunately i.MX RT does not support ECC RAM. Its SDRAM interface supports only 8-bit and 16-bit modes.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

1,063 次查看
scribble
Contributor I

Hi Victor, I was referring to the internal RAM, does this have any support?

0 项奖励
回复

1,063 次查看
b36401
NXP Employee
NXP Employee

i.MX RT does not support parity check on internal RAM too.
Sorry for the inconvenience.

0 项奖励
回复