I am trying test the LP SPI on the MIMXRT1060-EVKB Board, and I found that one of the SPI port is on the J17 connector, from the schematic there are DNP commented on the SPI lines.
Does that mean that I need to short R356, R350, R346 and R362 to make it work with the connector J17?
Thanks a lot for your help
已解决! 转到解答。
Hi Omar
Thanks for the confirmation, that is helpful.
I have one more question about the CAN testing:
According to the circuit, it needs the 10K pull up resister:
So is it OK that we just short the R269 and put the CAN_STBY to high by the MCU without putting 10K resister at R268?
I did this modification without connecting R268, drive the CAN_STBY to high by MCU.
And I cannot send CAN out successfully by running "flexcan_ping_pong_buffer_transfer" example. The MbStatusFlags are always 0 (IFLAG1 and IFLAG2).
So is pull up resister R 267 is a must? or something else might be wrong?
Thanks a lot for your help
Ni
Hi Omar
Thanks for the confirmation, that is helpful.
I have one more question about the CAN testing:
According to the circuit, it needs the 10K pull up resister:
So is it OK that we just short the R269 and put the CAN_STBY to high by the MCU without putting 10K resister at R268?
I did this modification without connecting R268, drive the CAN_STBY to high by MCU.
And I cannot send CAN out successfully by running "flexcan_ping_pong_buffer_transfer" example. The MbStatusFlags are always 0 (IFLAG1 and IFLAG2).
So is pull up resister R 267 is a must? or something else might be wrong?
Thanks a lot for your help
Ni