MIMXRT1050-EVK Error: Wire Ack Fault - target connected?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1050-EVK Error: Wire Ack Fault - target connected?

2,095 Views
OmarBengoa
Contributor II

Hi everybody.

I have a board MIMXRT1050-EVK with Display touch, I work with MCU Xpresso IDE 11.3.0.

Yesterday 02 March 2021 all worked fine, but this morning when connected the board to USB on my PC (Windows 10), the board is recognized in my PC correctly but new programs doesn't load on board and an error appears:

Error.png

 

 

 

Could you help me to resolved this issue?

Thanks.

Labels (1)
0 Kudos
Reply
5 Replies

1,878 Views
Sowmiya_R
Contributor I

Hi,

I am facing same error , could you please help me on this.

Sowmiya_R_0-1646981520935.png

 

0 Kudos
Reply

1,872 Views
yvzblgcyln
Contributor I

Hi,

My solution was just changing the direction of connection cable on NXP board between nxp board and LPC Link 2. Just reconnect cable on NXP board in the other direction.

I hope it works for you too. 

0 Kudos
Reply

1,940 Views
yvzblgcyln
Contributor I

hello sir, did you solve it?

0 Kudos
Reply

1,868 Views
Sowmiya_R
Contributor I

No , could not solve it. Can you suggest some other solution 

Tags (1)
0 Kudos
Reply

1,865 Views
yvzblgcyln
Contributor I

wops, sorry to heard that. I think there is no other way because i had tried everything, last thing i did was changing cable direction and it had worked for me.. btw i assume that you install all related driver so i wont say to you to install drivers.

0 Kudos
Reply