In the iMXRT spec, it states that if 50Mhz is used for the reference clock then placing a value of x9 in the MSCR register should provide the 2.5mhz MDC clock to the ethernet phy. Unfortunately, when I do that, I get a higher frequency around 7mhz. I measured the ref_clock and it was at 50mhz. Are there other dividers somewhere which affect this, or do I have some clocking mis-selected. I have to place a value of around 0x40 in the MSCR register to get the proper frequency.
Hi,
As the following pic, you can write the
ENET->MSCR&=~(0x3F<<1);
ENET->MSCR|=0x09<<1;
BTW, for your code, in the debugger, pls check the ENET->MSCR register and check if the MII_SPEED bits is 0x09.
Hope it can help you
BR
XiangJun Rong
Ok if I set MSCR register to 0x112, I get .14us clock or about 7mhz. The ref_clk is measured at .02us or 50mhz (measured with a scope). I would expect to get 2.5mhz out. I have to set MSCR to 0x140 in order to get the 2.5mhz.
Hi,
Pls try to use different MII_SPEED value and test the MDC clock frequency until it is 2.5MHz.
BR
XiangJun Rong