During porting of some code from i.MX1164 to i.MXRT1176, I have stumbled on a problem I could use some help on....
The project is done in Keil!
The (reduced) project implements USB (Bulk, not important). When I enable a specific piece of code, I get the L6244E error, the code (in usb_device_dci.c):
#if ((defined(USB_DEVICE_CONFIG_EHCI)) && (USB_DEVICE_CONFIG_EHCI > 0U))
/* EHCI device driver interface */
static const usb_device_controller_interface_struct_t s_UsbDeviceEhciInterface = {
USB_DeviceEhciInit, USB_DeviceEhciDeinit, USB_DeviceEhciSend,
USB_DeviceEhciRecv, USB_DeviceEhciCancel, USB_DeviceEhciControl};
#endif
The linker file:
#if (defined(__ram_vector_table__))
#define __ram_vector_table_size__ 0x00000400
#else
#define __ram_vector_table_size__ 0x00000000
#endif
#define m_flash_config_start 0x30000400
#define m_flash_config_size 0x00000C00
#define m_ivt_start 0x30001000
#define m_ivt_size 0x00001000
#define m_interrupts_start 0x30002000
#define m_interrupts_size 0x00000400
#define m_text_start 0x30002400
#define m_text_size 0x00FBDC00
#define m_qacode_start 0x00000000
#define m_qacode_size 0x00040000
#define m_interrupts_ram_start 0x20000000
#define m_interrupts_ram_size __ram_vector_table_size__
#define m_data_start (m_interrupts_ram_start + m_interrupts_ram_size)
#define m_data_size (0x00040000 - m_interrupts_ram_size)
#if (defined(__use_shmem__))
#define m_rpmsg_sh_mem_start 0x202C0000
#define m_rpmsg_sh_mem_size 0x00002000
#define m_data2_start 0x202C2000
#define m_data2_size 0x0007E000
#else
#define m_data2_start 0x202C0000
#define m_data2_size 0x00080000
#endif
#define m_core1_image_start 0x30FC0000
#define m_core1_image_size 0x00040000
/* Sizes */
#if (defined(__stack_size__))
#define Stack_Size __stack_size__
#else
#define Stack_Size 0x2000
#endif
#if (defined(__heap_size__))
#define Heap_Size __heap_size__
#else
#define Heap_Size 0x2000
#endif
#if defined(XIP_BOOT_HEADER_ENABLE) && (XIP_BOOT_HEADER_ENABLE == 1)
LR_m_text m_flash_config_start m_text_start+m_text_size-m_flash_config_start { ; load region size_region
RW_m_config_text m_flash_config_start FIXED m_flash_config_size { ; load address = execution address
* (.boot_hdr.conf, +FIRST)
}
RW_m_ivt_text m_ivt_start FIXED m_ivt_size { ; load address = execution address
* (.boot_hdr.ivt, +FIRST)
* (.boot_hdr.boot_data)
* (.boot_hdr.dcd_data)
}
#else
LR_m_text m_interrupts_start m_text_start+m_text_size-m_interrupts_start { ; load region size_region
#endif
VECTOR_ROM m_interrupts_start FIXED m_interrupts_size { ; load address = execution address
* (.isr_vector,+FIRST)
}
ER_m_text m_text_start FIXED m_text_size { ; load address = execution address
* (InRoot$$Sections)
.ANY (+RO)
}
#if (defined(__ram_vector_table__))
VECTOR_RAM m_interrupts_ram_start EMPTY m_interrupts_ram_size {
}
#else
VECTOR_RAM m_interrupts_start EMPTY 0 {
}
#endif
RW_m_data m_data_start m_data_size-Stack_Size-Heap_Size { ; RW data
.ANY (+RW +ZI)
* (RamFunction)
* (NonCacheable.init)
* (*NonCacheable)
}
ARM_LIB_HEAP +0 EMPTY Heap_Size { ; Heap region growing up
}
ARM_LIB_STACK m_data_start+m_data_size EMPTY -Stack_Size { ; Stack region growing down
}
#if (defined(__use_shmem__))
RW_m_ncache m_rpmsg_sh_mem_start EMPTY 0 {
}
RPMSG_SH_MEM m_rpmsg_sh_mem_start UNINIT m_rpmsg_sh_mem_size { ; Shared memory used by RPMSG
* (rpmsg_sh_mem_section)
}
RW_m_ncache_unused m_rpmsg_sh_mem_start+m_rpmsg_sh_mem_size EMPTY 0 { ; Empty region added for MPU configuration
}
#else
RW_m_ram_text m_qacode_start m_qacode_size { ;
* (CodeQuickAccess)
}
RW_m_ncache m_data2_start EMPTY 0 {
}
RW_m_ncache_unused +0 EMPTY m_data2_size-ImageLength(RW_m_ncache) { ; Empty region added for MPU configuration
}
#endif
}
LR_CORE1_IMAGE m_core1_image_start {
CORE1_REGION m_core1_image_start m_core1_image_size {
*(*core1_code)
}
}
The specific error from the linker:
flexspi_nor_debug\Application.out: Error: L6244E: Load region LR_m_text address (0x30000400) not aligned on a 2048 byte boundary.
If I specifically change in the linker file:
#define m_flash_config_start 0x30000400
to
#define m_flash_config_start 0x30000800
The error goes away, but the code will (obviously) not work as the address is wrong.
What am I missing in this ???
Hi @carstengroen,
It is hard to say. I believe this error is from the ARM compiler toolchain, so I would highly recommend you to go to their forums for a better support.
BR,
Edwin.
Yes, this is ARM compiler chain.
Also asked the question on Keil forum, so far no solution. I was just hoping that someone here did experience the same problem.
(I have the code running by using --legacyalign in linker settings, but this is deprecated so not a future proof solution)