Issue with creating bootable image for RT-1050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Issue with creating bootable image for RT-1050

1,099 次查看
bzhang3
Contributor I

Hello All,

 

I'm using Keil IDE to build code to execute from the hyperflash on the RT1050 EVKB. When I load the code onto flash and run in the Keil debugger, everything works fine. And when I close the debugger and power cycle the board, code still executes successfully from flash.

 

Now I'm trying to build a bootable image and use the MFGTool to load code onto the H-flash. I'm running into issues. Here's steps I followed:

 

1. Creating a s-record file with the .axf generated by Keil (test.axf and test.srec attached):

      "fromelf --m32combined --output=test.srec test.axf"

 

2. Creating binary file with elftosb:

      "elftosb.exe -f imx -V -c imx-flexspinor-normal-unsigned.bd -o test.bin test.srec"

 

The output test.bin only has 0 bytes. However if I use the led demo in the example images of the FlashLoader, I can generate a .bin file successfully. 

 

Can anybody help me figure out what the problem is? Many thanks in advance. 

 

Regards,

Bin

标签 (1)
0 项奖励
回复
0 回复数