About the datasheet of R1060

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the datasheet of R1060

1,589 Views
wangtiegang
Contributor II

I read the dadasheet abou R1060

It was said that have two 10M/100M ethernet port, but only find in factsheet.

In the reference manual and even the evaluation board , I don't find any information about  two 10M/100M ethernet ports. 

How the two ethernet ports working ?

Any information in detail ?

0 Kudos
Reply
2 Replies

1,434 Views
igorpadykov
NXP Employee
NXP Employee

Hi 铁钢 王 

for ENET2 please refer to references in Table 3-2. CM7 domain interrupt summary

i.MX RT1060 Processor Reference Manual

https://www.nxp.com/docs/en/reference-manual/IMXRT1060RM.pdf 


Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,434 Views
wangtiegang
Contributor II

what's the relationship of  two ethernet ports.?

Independt ?

      RT1060

      |          |

enet1     enet2

or like this

       RT1060

            | 

        switch

            |

    |------|----|

enet1     enet2

0 Kudos
Reply