Internal flash on RT 1064 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Internal flash on RT 1064 ?

ソリューションへジャンプ
2,654件の閲覧回数
carstengroen
Senior Contributor II

I have the EVK 1064 which runs just fine. I'm in the process of designing my first board with the RT 1064, and in that process I have a hard time finding info on the internal (QSPI?) Flash. On the EVK, I have the Flash at 0x70000000 and according to the UM this is FlexSPI2 interface. Is that connected to the internal flash of the CPU, or is this the external flash (on the EVK) ?

What pins on the CPU is used (I assume that some of the pins are connected both to external pins as well as the internal Flash chip) ?

I have not (yet) been able to find info on the internal flash in the manuals so far...

1 解決策
2,052件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Carsten

info on the internal flash can be found in

AN12290 Migration Guide from i.MX RT1060 to i.MX RT1064

https://www.nxp.com/docs/en/application-note/AN12290.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,052件の閲覧回数
jay_heng
NXP Employee
NXP Employee
0 件の賞賛
返信
2,053件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Carsten

info on the internal flash can be found in

AN12290 Migration Guide from i.MX RT1060 to i.MX RT1064

https://www.nxp.com/docs/en/application-note/AN12290.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,052件の閲覧回数
carstengroen
Senior Contributor II

Thanks a lot Igor!

I don't quite know how that document slipped my eyes in the first place :smileyhappy:

Thanks!

0 件の賞賛
返信