IMXRT1052 SPDIF txClkSource tx_clk1 (from SAI1) not work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1052 SPDIF txClkSource tx_clk1 (from SAI1) not work

Jump to solution
1,481 Views
vega_sdr
Contributor I

Hi !

With XTALOSC and SPDIF0_CLK_ROOT clock source SPDIF transmitter work fine.

But when I select spdif_config.txClkSource = 2U//txClk from SAI1 for SPDIF, SPDIF not work.

SAI1 clock source - audiopll or ext mclk, I see all clock and data on SAI1 pins.

0 Kudos
Reply
1 Solution
1,464 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @vega_sdr ,

   Seems my previous understanding is not correct. It is not the SAI ROOT clock, it is the sai rxbclk.

kerryzhou_0-1626846686077.png

kerryzhou_1-1626846700947.png

 

2 is the txclk1, from the above picture, it is the rxbclk.

So, do you check the RXBCLK, whether that have wave or not?

Best Regards,

kerry

 

View solution in original post

0 Kudos
Reply
6 Replies
1,457 Views
vega_sdr
Contributor I

Thanks a lot !

My mistake was that I didn't activate synchronous mode for sai_rx (I2S_RCR2_SYNC bit), in my project I use only sai_tx.

 

0 Kudos
Reply
1,452 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Thanks for your updated information.

So, if you don't use SAI rx, it's better your SPDIF still use the SPDIF clock source :SPDIF0_CLK_ROOT.

Best Regards,

Kerry

0 Kudos
Reply
1,450 Views
vega_sdr
Contributor I

SAI1 and SPDIF must use external clock, but on my pcb it traced only to SAI1_mclk pin.

0 Kudos
Reply
1,472 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @vega_sdr 

  Do you configure the same sai1 clock to your SPDF0_CLK clock?

kerryzhou_0-1626835924686.png

I mean, set your SAI1 clock the same frequency to your working SPDIF0_CLK_ROOT, whether this method works or not?

You can use the mcuxpresso project, cfg tool to configure the clock directly to test it.

Best Regards,

Kerry

 

0 Kudos
Reply
1,467 Views
vega_sdr
Contributor I

I set same clockPLL4_MAIN_CLK for SAI1_CLK and for SPDF0_CLK.

SPDIF work  when spdif_config.txClkSource = 1 and not work when spdif_config.txClkSource = 2

0 Kudos
Reply
1,465 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @vega_sdr ,

   Seems my previous understanding is not correct. It is not the SAI ROOT clock, it is the sai rxbclk.

kerryzhou_0-1626846686077.png

kerryzhou_1-1626846700947.png

 

2 is the txclk1, from the above picture, it is the rxbclk.

So, do you check the RXBCLK, whether that have wave or not?

Best Regards,

kerry

 

0 Kudos
Reply