Hi !
With XTALOSC and SPDIF0_CLK_ROOT clock source SPDIF transmitter work fine.
But when I select spdif_config.txClkSource = 2U//txClk from SAI1 for SPDIF, SPDIF not work.
SAI1 clock source - audiopll or ext mclk, I see all clock and data on SAI1 pins.
解決済! 解決策の投稿を見る。
Hi @vega_sdr ,
Seems my previous understanding is not correct. It is not the SAI ROOT clock, it is the sai rxbclk.
2 is the txclk1, from the above picture, it is the rxbclk.
So, do you check the RXBCLK, whether that have wave or not?
Best Regards,
kerry
Thanks a lot !
My mistake was that I didn't activate synchronous mode for sai_rx (I2S_RCR2_SYNC bit), in my project I use only sai_tx.
Thanks for your updated information.
So, if you don't use SAI rx, it's better your SPDIF still use the SPDIF clock source :SPDIF0_CLK_ROOT.
Best Regards,
Kerry
SAI1 and SPDIF must use external clock, but on my pcb it traced only to SAI1_mclk pin.
Hi @vega_sdr
Do you configure the same sai1 clock to your SPDF0_CLK clock?
I mean, set your SAI1 clock the same frequency to your working SPDIF0_CLK_ROOT, whether this method works or not?
You can use the mcuxpresso project, cfg tool to configure the clock directly to test it.
Best Regards,
Kerry
I set same clockPLL4_MAIN_CLK for SAI1_CLK and for SPDF0_CLK.
SPDIF work when spdif_config.txClkSource = 1 and not work when spdif_config.txClkSource = 2
Hi @vega_sdr ,
Seems my previous understanding is not correct. It is not the SAI ROOT clock, it is the sai rxbclk.
2 is the txclk1, from the above picture, it is the rxbclk.
So, do you check the RXBCLK, whether that have wave or not?
Best Regards,
kerry