IMXRT1024 LPUART Transmit Data Register in Fugire

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMXRT1024 LPUART Transmit Data Register in Fugire

Jump to solution
1,054 Views
Lukas_Frank
Senior Contributor I

Hi all,

Where is the DATA Register mentioned in IMXRT1024 Reference Manual Section 44.3.4? What is the representation of it in Figure 44-1?

Lukas_Frank_0-1625656524237.png

 

Thanks and Regards.

 

0 Kudos
Reply
1 Solution
1,027 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Lukas_Frank,

As it  mention in the UM: Programs store data into the transmit FIFO by writing to the DATA register so it should be before at some point in the FIFO but more detailed information is not available.

Best Regards,

Alexis Andalon

View solution in original post

3 Replies
1,046 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Lukas_Frank,

Unfortunately, the block diagram in the RM is only a visual representation and more detailed information is not available.

Best Regards,

Alexis Andalon

1,036 Views
Lukas_Frank
Senior Contributor I

How it can be possible. There is a term in reference manual. But, there is not representation of it. What is the way for accesing more clear way?

Thanks and Regards. 

0 Kudos
Reply
1,028 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Hello @Lukas_Frank,

As it  mention in the UM: Programs store data into the transmit FIFO by writing to the DATA register so it should be before at some point in the FIFO but more detailed information is not available.

Best Regards,

Alexis Andalon