Hi Sir
I have two question to confirm.
1. Is IMX6Q PCIE supporting MSI-X interrupt ? If yes,how many interrupt it supports?
2. How many PCIE BAR IMX6Q supports? And the size of each BAR.
Thanks
Hi yong
MSI-X is supported acording to Table 48-2. Core Interface Summary i.MX6DQ Reference Manual,
for bar details one can check
Driver access PCIE Device via IO port failed with IMX6
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------