IMX RT1060 FLEXPWM2_EXT_CLK external clock maximum input frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX RT1060 FLEXPWM2_EXT_CLK external clock maximum input frequency

跳至解决方案
1,206 次查看
kinlee
Contributor II

Hi

I want to use an external clock for a PWM signal. I understand that this external clock will be routed through XBAR, and in my case XBAR1_OUT48 is connected to FLEXPWM2_EXT_CLK.

However what is the maximum frequency I can drive FLEXPWMn_EXT_CLK. Is it stated in any documentation? 

best regards

KL

0 项奖励
回复
1 解答
1,166 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @kinlee 

 

I would like to apologize for the delay. We are overloaded on the request these days. I really really appreciate that you were so patient.

 

Regarding your question about the EXT_CLK for FlexPWM2, after double-checking internally, this external clock only can reach to the half of internal ipg_clock, that its default is 150MHz, so the maximum frequency you can drive on FLEXPWMn_EXT_CLK is 75MHz. Sadly, It is not stated in any public documentation.

 

Please let me know if you have more questions.

 

Best Regards.
Pablo Avalos.

在原帖中查看解决方案

1 回复
1,167 次查看
PabloAvalos
NXP TechSupport
NXP TechSupport

Hi @kinlee 

 

I would like to apologize for the delay. We are overloaded on the request these days. I really really appreciate that you were so patient.

 

Regarding your question about the EXT_CLK for FlexPWM2, after double-checking internally, this external clock only can reach to the half of internal ipg_clock, that its default is 150MHz, so the maximum frequency you can drive on FLEXPWMn_EXT_CLK is 75MHz. Sadly, It is not stated in any public documentation.

 

Please let me know if you have more questions.

 

Best Regards.
Pablo Avalos.