Now I trying to output FlexPWM1 pulses with fixed number.
IOMUXC_GPIO_SD_B0_00_FLEXPWM1_PWMA00
IOMUXC_GPIO_SD_B0_01_FLEXPWM1_PWMB00
In SDK, QTMR example has DMA solution.
But, I can not solve this issue.
Is there another process ?
已解决! 转到解答。
If I understood correctly, you want the source address to change and sweep through all of the period array, while maintaining the destination address on the same place (the same peripheral address). Is this correct? This can be done by following the implementation described on Section "6.4.4.1 Single Request" of the Reference Manual, but modifying the SLAST register to prevent it from resetting after each major loop transfer. Note that this implementation would have to include a piece of code that makes sure that the source address does not exceed the maximum address of the period array, but that would be the only detail to keep in mind.
I hope this helps,
Edwin.
Hi @shingofujiwara,
The RT106x SDK should come with a non dma version of the qtmr implementation for output pwm (qtmr_inputcapture_outputpwm), as well as other implementation of a PWM which would also be helpful for your inquiry. Could you please specify which SDK example code you are basing your application on?
BR,
Edwin.
Thanks. @EdwinHz ,
Now I based on "driver_examples\pwm" project.
And combined "driver_examples\qtmr\inputcapture_outputpwm_dma" project.
In qtmr_dma project, DMA transfer period data to compare counter. (2byte width, 2byte length, 1 count)
I want to transfer period to compare register for defined cycles.
I prepared "uint16_t period_array[100]" for DMA transfer to compare register.
How can I use DMA, transfer incremental memory address to same peripheral address ?
If I understood correctly, you want the source address to change and sweep through all of the period array, while maintaining the destination address on the same place (the same peripheral address). Is this correct? This can be done by following the implementation described on Section "6.4.4.1 Single Request" of the Reference Manual, but modifying the SLAST register to prevent it from resetting after each major loop transfer. Note that this implementation would have to include a piece of code that makes sure that the source address does not exceed the maximum address of the period array, but that would be the only detail to keep in mind.
I hope this helps,
Edwin.
Thanks @EdwinHz
So, now I can transfer period value to PWM register.
But, pulse width does not change.
Only set value to VAL register, does not update internal buffer ?
It need to set LDOK register ?
And, DMA does not transfer 0x0000 to VAL register ?
I thought that I can stop PWM (keep High or Low) by transfer 0x00 to VAL register.
How about this ?