Hi All,
I want to configure SAI2 in sln-local2-iot which is connected to DMIC in evk board as an interface for the communication with the host processor as follows.
Pinmuxing is done as follows.
SAI2_TX_DATA - GPIO_AD_B0_09-Jtag TDI pin
SAI2_TX_BCLK - GPIO_AD_B0_05-Boot pin
SAI2_TX_SYNC - GPIO_AD_B0_04-Boot pin
SAI2_RX_DATA - GPIO_AD_B0_08 - DMIC pin
I Tried to record DMIC data from SAI1 using SLN_AMP_Write() in the host processor via SAI2 .But data is not coming out of the TX_DATA pin. Only BCLK and FYNC is coming. I am also using Jtag for debugging.Is that making any issue ?Could you please help me to figure out the issue?What all configuration is needed for the SAI2 to communicate with the host processor?
Hi @Blackpearl ,
As this case is no updated information for 1 month.
If you have any questions, please create the new case, we can talk it in your new case.
As we can't open the case more than one month, this case is opened for 2 month.
Thanks a lot for your understanding.
Best Regards,
Kerry
Hi @kerryzhou ,
Thanks for the response. I will open this as a new case.