After working on PXP for some time, an IRQ interrupt cannot be received.
When an exception occurs, the registers are as follows
Errors occur with several characteristics:
1. BLOCKX and BLOCKY always is 1,this value is variable during normal operation;
2. IRQ intterupt will not trigger;
3. When error occurring,turn on and then trun off SFTRST bit for softreset PXP,it cannot resume normal operation .
Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
I was wondering if you can illustrates the testing steps that can replicate the issue, as I'd like to get more infromation.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Environment: 8M flash XIP, 32M SDRAM
Using 800*480 LCD(ARGB8888) to display GUI,and use pxp to achieve blend and rotate operation frequently;
after 1-3 hours long time work, PXP will work abnormal as described above.
Hi,
Thanks for your reply.
Whether you can replicate the phenomenon on the MIMXRT1050-EVK board, If yes, please share the code, then I can give it a try.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------