Frame rate issue with 800x600 LCD

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Frame rate issue with 800x600 LCD

969 Views
oliviermonnom
Contributor II

Hi,

I've a MIMXRT1064-EVK board and the LCD (480*272 pix) display.

I've a PAL camera and an CCIR656 encoder whose outputs go directly to the CSI interface. DATA flux is about 27MB/s.

I've modified slightly the demo prg to deal with the camera, so far so good, works fine.

Then I changed the LCD for a 800x600pix (with a // to LVDS converter) and I'm facing framerate issue (no more 25fps for the CAM).

Here is the question: is there somewhere a calculation (at least theoretical) of the max resolution possible for a (decent) framerate of 25Hz with the RT10xx and it's associated SDRAM?

Thank you,

Olivier

Labels (2)
0 Kudos
Reply
1 Reply

873 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Olivier Monnom,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Here is the question: is there somewhere a calculation (at least theoretical) of the max resolution possible for a (decent) framerate of 25Hz with the RT10xx and it's associated SDRAM?
-- Whether you like to know which color space format is appropriate for the 25 fps, if yes, I think RGB888 is a good choice.

TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply