Fault on backlight circuit of MIMXRT1050-EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Fault on backlight circuit of MIMXRT1050-EVK

1,183 次查看
abertu
Contributor II

I have done some climatic test using the dev-board MIMXRT1050-EVK.
After few hours I have stopped because I my TFT was off.
I have found U8 (UM1661) hot and C88 (4.7 uH, 6.3 V) in shortcircuit.
The rated voltage of the capacitor is not enough to be used for the backlight circuit, it's required at least a 25 V.

标记 (2)
0 项奖励
回复
1 回复

1,018 次查看
Carlos_Musich
NXP Employee
NXP Employee

Hi Angelo,

thank you for your input. I will report it to the appropriate team so they can examine this case.

Reards,

Carlos

0 项奖励
回复