I am trying to flash the code to iMX RT 1170 Evk using NXP MCU Boot utility. But I cannot find the USB HID device. Event though i followed the steps on
https://github.com/JayHeng/NXP-MCUBootUtility
Also I have checked with boot switches setting.
Please can anyone help me ?
Thanks in advance!
Hello
Hope you are well.
How are you powering the EVK? If you are using the barrel connector(J43) make sure that that jumpers in J38 is in default position(1-2). If you want to power from the Freelink interface(J11) the jumper must be in position 5-6.
The USB interface for serial download is USB1, make sure you are using the correct interface:
Also, the SW1[3-4] need to be in position 01 for serial downloader.
If you have more questions do not hesitate to ask me.
Best regards,
Omar