Facing issue with LPC Link 2 with iMX RT 1170 Evk

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Facing issue with LPC Link 2 with iMX RT 1170 Evk

1,290件の閲覧回数
Ankush_9881
Contributor II

I am trying to flash the code to iMX RT 1170 Evk using NXP MCU Boot utility. But I cannot find the USB HID device. Event though i followed the steps on

https://github.com/JayHeng/NXP-MCUBootUtility

Also I have checked with boot switches setting. 

Please can anyone help me ?

Thanks in advance!

0 件の賞賛
返信
2 返答(返信)

1,270件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
Hope you are well.

How are you powering the EVK? If you are using the barrel connector(J43) make sure that that jumpers in J38 is in default position(1-2). If you want to power from the Freelink interface(J11) the jumper must be in position 5-6.

The USB interface for serial download is USB1, make sure you are using the correct interface:

Omar_Anguiano_0-1643671892537.png

 

Also, the SW1[3-4] need to be in position 01 for serial downloader.

If you have more questions do not hesitate to ask me.
Best regards,
Omar

1,254件の閲覧回数
Ankush_9881
Contributor II

Thank you very much for the solution!

0 件の賞賛
返信