Hello,
I am building my own module to access an external flash memory using a MIMXRT1061CVL5B controller. It is built on the example in the SDK flexspi_nor_polling_transfer, I keep running into a hardfault that is caused by the FLEXSPI_Init, and I am almost sure it is from the function call FLEXSPI_SoftwareReset.
I tried to add the object files to the RAM in the .icf file as it is in the SDK example but that didn't help
Can anybody help me?
Thanks in advance.
已解决! 转到解答。
Hi @Lukaz ,
Ok, I know, your issue is caused by other code, eg, PIT.
I think you enable the PIT interrupt, right?
This should be the key point, when do the flash operation, it should not be interrupted by other moduld, so you need to disable the PIT interrupt before you do the flexSPI operation, after it is finished, you can enable the PIT interrupt again.
Please help to check it, I think it is root reason.
Best Regards,
kerry
Hi @Lukaz ,
Thank you for your interest in the NXP MIMXRT product, I would like to provide service for you.
flexspi_nor_polling_transfer is used to the external flash is QSPI flash, in fact, it is for: IS25WP064AJBLE.
So, in your own RT1061 board, which detail flash you are using now? Different external flash have different configuration.
Even you use the same qspi flash IS25WP064AJBLE, in the first time, as your QSPI flash is new, and QE bit is not enabled, you need to run it from internal flash, otherwise, you will meet the boot issues.
If you use other flash, you also meet issues.
So, at first, please let us know your used external flash, and the connection to the RT1061 board.
Best Regards,
Kerry
Hello Kerry,
I am aware of the difference between the flashes. I am using winbond W25Q64JVSSIQ, and I am able to boot from it with no problem. The QE bit is by default enabled (actually can't be cleared in this flash). Can you please give an example of how could the configuration for the initialization be different? I customized all my functions and the LUT to be compatible with the flash I am using, only the initialization is the same as the one in the flexspi_nor_polling_transfer example. Please see below my init function.
Hi @Lukaz ,
Thanks for your updated information.
Now, run this code in the internal RAM:
SDK_2_12_0_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\flexspi\nor\polling_transfer
You need to modify the code for your winbond chip:
1. Modify LUT
1). From:
/* Erase Sector */
[4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xD7, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
To:
/* Erase Sector */
[4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0X20, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),
2). From
/* Enable Quad mode */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x01, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04),
to:
/* Enable Quad mode */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x31, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04),
3) QE bit
app.h
From
#define FLASH_QUAD_ENABLE 0x40
to:
#define FLASH_QUAD_ENABLE 0x02
2. Please also check your hardware
DQS pin, I mean this pin:
GPIO_SD_B1_05
You need to leave it as float, otherwise, it will influence the flexSPI frequency.
Then test the code in the RAM, whether you can do the external flash erase, read, write or not?
Best Regards,
Kerry
Hi @Lukaz ,
Thanks very easy if you are using the MCUXPresso IDE, just do the following configuration:
I need to use the RAM code to test your external flash totally works at first.
You can check the printf information with the UART, or you can check it in console if you enable the semihost:
Please test it on your side, and share me your printf information after the code modification.
Please also make sure the DQS pin is float, otherwise, you need to cut down the flexSPI frequency to 60Mhz, and set :
Dummy read strobe generated by FlexSPI controller and looped back internally
(FlexSPIn_MCR0[RXCLKSRC] = 0x0)
Best Regards
Kerry
Hi @Lukaz ,
Good!
So, from your printf log, you are totally works OK.
So, it already pass the the software reset you mentioned.
Please help to check it, I think your issue is solved now.
If you still have issues, just kindly let me know.
Best Regards,
Kerry
Hi Kerry
Thank you for your help, that is what I exactly thought that the issue is now solved, but it wasn't.
I could track it tho and I know now what is causing this hardfault, but I don't know why.
In my project I use the PIT module as well, I kept tracking things in my project and long story short, when I eliminate the PIT initialization from the project everything works fine otherwise I keep running into the hardfault. If you have some idea about why that might be so, I would be grateful.
Thanks in advance.
Hi @Lukaz ,
Ok, I know, your issue is caused by other code, eg, PIT.
I think you enable the PIT interrupt, right?
This should be the key point, when do the flash operation, it should not be interrupted by other moduld, so you need to disable the PIT interrupt before you do the flexSPI operation, after it is finished, you can enable the PIT interrupt again.
Please help to check it, I think it is root reason.
Best Regards,
kerry
Hi Kerry,
I have one more question please, does this mean when I start any flash operation I should disable all interrupts from other modules? would that be solved if I use the DMA for flash operations?
Hi @Lukaz ,
Set the flash as the highest level, otherwise, it may meet issues when other interrupt happens.
BTW, you also can use this ROM API:
SDK_2_12_0_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\fsl_romapi
Then check, whether it can be influenced by other interrupt.
This code also can do the flash operation, with the ROM API code.
Best Regards,
Kerry