Empty frame received (RT1176)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Empty frame received (RT1176)

382 Views
luk1
Contributor I

Ethernet receives data for a period of time and then fails to receive new data.The " ENET_GetRxFrameSize "show that the length of the received frame is 0. The ' control ' element of the ' curBuffDescrip ' always comes as 0x8000 and as a result ' kStatus_ENET_RxFrameEmpty ' is returned.At this time, if the network driver is re-initialized, data reception can return to normal. What could be the reason for this situation?

My board is based on the RT1176 development, using the SDK 2.11.

0 Kudos
Reply
1 Reply

335 Views
Pablo_Ramos
NXP Employee
NXP Employee

Hi @luk1,

Thank you for getting in touch, I apologize for the delay

To narrow down the issue, could you please help me test with the latest version of SDK v15.1, select an example closer to your application, and share the results with me?

Please inform me if you have any additional information about your application or if you discover anything new during this time

0 Kudos
Reply