I am having an issue where if I SetPinMux on GPIO_EMC_39_ENET2_MDIO on an iMXRT1062, the system crashes. Is there some interaction with some other module or pin that is used that would cause this? I need to use both MACs independently for two LAN ports.
Solved! Go to Solution.
Please refer to this post:
Also note, you can share one management interface (MDC/MDIO) between the 2 ethernet interfaces, you just need to set a different address on the PHY.
-Nick
Please refer to this post:
Also note, you can share one management interface (MDC/MDIO) between the 2 ethernet interfaces, you just need to set a different address on the PHY.
-Nick
See this thread for an explanation:
Also note, you can share one management interface (MDC/MDIO) between the two ethernet interfaces, you need to set a different address on the PHY.
-Nick
Do you know what the base address is for the ENET management interface? Could not find it in the reference manual and need it for device tree.