ENET2 MDIO pin conflict

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ENET2 MDIO pin conflict

跳至解决方案
1,731 次查看
jautry
Contributor IV

I am having an issue where if I SetPinMux on GPIO_EMC_39_ENET2_MDIO on an iMXRT1062, the system crashes.  Is there some interaction with some other module or pin that is used that would cause this?  I need to use both MACs independently for two LAN ports.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,720 次查看
nickwallis
Senior Contributor I

Please refer to this post:

https://community.nxp.com/t5/i-MX-RT/target-crashes-writing-to-register-SW-MUX-CTL-PAD-GPIO-SD-B1-05...

Also note, you can share one management interface (MDC/MDIO) between the 2 ethernet interfaces, you just need to set a different address on the PHY.

-Nick

在原帖中查看解决方案

0 项奖励
回复
3 回复数
1,721 次查看
nickwallis
Senior Contributor I

Please refer to this post:

https://community.nxp.com/t5/i-MX-RT/target-crashes-writing-to-register-SW-MUX-CTL-PAD-GPIO-SD-B1-05...

Also note, you can share one management interface (MDC/MDIO) between the 2 ethernet interfaces, you just need to set a different address on the PHY.

-Nick

0 项奖励
回复
1,712 次查看
nickwallis
Senior Contributor I

See this thread for an explanation:

https://community.nxp.com/t5/i-MX-RT/target-crashes-writing-to-register-SW-MUX-CTL-PAD-GPIO-SD-B1-05...

Also note, you can share one management interface (MDC/MDIO) between the two ethernet interfaces, you need to set a different address on the PHY.

-Nick

0 项奖励
回复
1,674 次查看
jautry
Contributor IV

Do you know what the base address is for the ENET management interface?  Could not find it in the reference manual and need it for device tree.

标记 (1)
0 项奖励
回复