Does RT 1052/1050 support hard ware FIR filter

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does RT 1052/1050 support hard ware FIR filter

1,174 Views
zhangjiansheng
Contributor II

Hi,

Does RT 1050/1052 have the function of doing FIR/IIR filter function? 

Our current project using the RT 1050/1052 to capture the ECG signal and process. The ECG data need be filtered with FIR multiband filter and 50/60 hz notch filter. I want to know if RT 1052/1050 hard ware support the filter in the hardware level. And if there is any sample code or library for this?

Labels (1)
0 Kudos
Reply
1 Reply

1,047 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

Regarding hardware implementation of digital filters, you could refer to CMSIS-DSP software library.

On the MCUXpresso SDK, there are included some CMSIS-related examples.

Regarding EKG implementation (with software FIR filters), you could take a look at the following links:

https://www.nxp.com/pages/electrocardiograph-development-kit-for-tower-system:MED-EKG

https://www.nxp.com/docs/en/application-note/AN4323.pdf

https://www.nxp.com/docs/en/application-note/AN4644.pdf


Hope this will be useful for you.
Best regards!
/Carlos
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply