DCDC in i.MX RT1060

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DCDC in i.MX RT1060

1,772件の閲覧回数
er_arpit_arora
Contributor III

Hello NXP, I have a question regarding the DCDC module in i.MX RT1060. I've tried going through the datasheet, reference document, schematic and hardware development guide but I am not able to find any good documentation around the various inputs and outputs of the DCDC module.

Question: What is the purpose of the various pins? Could someone please explain in 1 or 2 sentences for each pin?

DCDC_IN_1

DCDC_IN_2

DCDC_IN_Q

DCDC_LP_1

DCDC_LP_2

DCDC_PSWITCH

DCDC_SENSE

タグ(2)
0 件の賞賛
返信
3 返答(返信)

1,564件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

You may refer to the DCDC block diagram as the reference manual.Hope it help you.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,564件の閲覧回数
er_arpit_arora
Contributor III

Hi Fang, thanks for your reply. I did go through all the documentation but I am afraid, it does not at all cover all the DCDC module pins. For example, there is no explanation of DCDC_IN_Q and DCDC_SENSE pins. Could you please explain the purpose of DCDC_IN_Q and DCDC_SENSE please?

0 件の賞賛
返信

1,564件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

You are welcome. DCDC_SENSE is for checking the output voltage. DCDC_IN_Q is one of the power for DCDC.

0 件の賞賛
返信