Hi,
I am a beginner working with the RT1170 microcontroller, and I'm using MCUXpresso as my development environment. I have a Quectel EC200U LTE module connected to the controller, and the communication is set up to occur through USB OTG2. I want to send AT commands to the LTE module and receive responses via USB. Could anyone guide me on how to send AT commands through USB? Any assistance would be greatly appreciated. Thanks in advance.
Hello
This application note might be helpful as it connects to the module using AT commands with USB: Connect i.MX RT1060 to USB 4G Module (RNDIS Mode) (nxp.com)
Best regards,
Omar