Hi community ,
we are using IMX RT 1020 for our next design and we just want to know if there is any provision to read all the 16 inputs i.e (DC1_IN0 to ADC1_IN15 ) with a single trigger .
Here are the available ADC selection , in 24 proposed ADCs we can use only 19 , 16 from ADC 1 and 3 from ADC 2
If there is any provision to read all the 16 sensors data connected to 16 ADCs of the MCU in one shot please let me know since reading individual input is a time taking process and includes latency
Thanks and Regards
Naren chandra
Hi Naren chandra ,
This post is totally the same as your another post:
Can we read all the ADC inputs in a channel with a single trigger ?
I already reply you in that post.
So, if you still have questions about it, please reply me in your another post directly.
Have a great day,
Kerry
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------