Can bus example on iMXRT1170-EVKB board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can bus example on iMXRT1170-EVKB board

Jump to solution
1,059 Views
nickager
Contributor II

Hi,

I'm struggling to get one of  the CAN examples on my IMXRT1170-EVKB board to send messages over CAN bus.

On the board I've connected CAN3 to a local test CAN bus going into a Teensy via a CAN transceiver with termination resistors. I am monitoring the RX and TX signals on the Teensy via a logic analyser. I ensure that the bus speed matches at both ends (1Mb/s)

I've tried various examples for example "evkbmimxrt1170_flexcan_interrupt_transfer_cm7". When I run the example I see:

* A breakpoint set in the interrupt "flexcan_callback" is never hit.

* After selecting node "a" the code is stuck in the while (!txComplete) - which never completes as "txComplete" is set in the interrupt which is never called.

* I don't see any signals on the logic analyser.

* However, if I swap the IMXRT1170-EVKB for an IMXRT1064-EVK board I have and use the same example, the message is sent successfully.  I see the message arrive in the Teensy, appear on the logic analyser and the breakpoint is hit in the interrupt routine. So I don't think its my hardware setup.

Any thoughts about what could be wrong and how to debug further.

Thanks

Nick

Tags (2)
0 Kudos
Reply
1 Solution
999 Views
nickager
Contributor II

For anyone that might suffer similar difficulties in the future the solution is to "Remove J102 and J103 jumpers.". I found this in the docs/readme.md associated with the CAN example ... I should have read the manual!

 

View solution in original post

0 Kudos
Reply
6 Replies
1,000 Views
nickager
Contributor II

For anyone that might suffer similar difficulties in the future the solution is to "Remove J102 and J103 jumpers.". I found this in the docs/readme.md associated with the CAN example ... I should have read the manual!

 

0 Kudos
Reply
555 Views
dipalipatil21212313
Contributor I
we face same issue and also try by removing jumpers j102 and j103 still not working
0 Kudos
Reply
425 Views
dipalipatil21212313
Contributor I
Hi,

I'm struggling to get one of the CAN examples on my IMXRT1170-EVKB board Transmit code is completed without interrupt ,but reception is not completed with or without interrupt,i have fallowing the same process as like transmitions.
0 Kudos
Reply
541 Views
nickager
Contributor II

Can you explain a little more about your setup. The setup that works for me is:
* From MCUXpresso choose "import SDK example" and select "canfd_interrupt_transfer_cm7"
* Connect CANH and CANL to CAN3 header - J47 see attached image

* Connect another board to receive/transmit on CAN id: 0x123 or 0x321 (see sample), ensure the CAN data rate is setup identically at both ends
* Connect a logic analyser to monitor what is happening on the CAN bus
* Stick a break point in the code sample interrupt routine.
* Run the sample.
* Observe the message in the logic analyser and see the break point being hit in the interrupt routine.

Hope this helps

Nick 

0 Kudos
Reply
520 Views
dipalipatil21212313
Contributor I
i have used same setup but its not working

0 Kudos
Reply
536 Views
nickager
Contributor II

Here's the image I meant to attach

0 Kudos
Reply