Can I use mimxrt1020 to debug new hardware?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use mimxrt1020 to debug new hardware?

766 Views
estacey
Contributor III

I've been told old evaluation boards have provided a way for re-purposing the board to use the on board debugging capability for the new hardware.  Does the mimxrt1020 provide such a feature?  It isn't mentioned in the hardware user manual.

Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

699 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Ellen Stacey,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Does the mimxrt1020 provide such a feature?
-- No, I'm afraid not.
Hope this is clear.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply