Can I use external Static RAM with i.MXRT1050? I need more Static RAM with battery backup

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can I use external Static RAM with i.MXRT1050? I need more Static RAM with battery backup

1,362 次查看
Soos
Contributor III

Is it possible to use external static RAM with iMXRT1050 ?

I need more battery backed-up RAM for our application.

标记 (1)
2 回复数

1,256 次查看
Yuri
NXP Employee
NXP Employee

Hello,

 

  The SEMC of the RT1050 supports devices with general purpose SRAM-like
interface.


Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,256 次查看
Soos
Contributor III

OK Thanks

I will use SEMC_CSX0 as CS for my Static RAM.