About low power mode on mxrt1021

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

About low power mode on mxrt1021

1,033 次查看
hiro8235
Contributor I

Can the low power mode be enabled with an empty ROM?
If so, is there a description of the settings in the IMXRT1021RM?
For example, system idle mode settings.
Thank you.

标签 (1)
0 项奖励
回复
3 回复数

1,027 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @hiro8235 

   low power mode enter need to use the code, you can download it to the internal RAM instead of the external flash, I think your mentioned empty ROM is no code in the external flash, right?

   If yes, you can download this SDK code to the RAM, just not do the POR, the low power code will help you enter the low power mode.

\SDK_2_11_0_EVK-MIMXRT1020\boards\evkmimxrt1020\demo_apps\power_mode_switch

SDK download link is:

https://mcuxpresso.nxp.com/en/builder?hw=EVK-MIMXRT1020

 

Wish it helps you!

Best Regards,

Kerry

0 项奖励
回复

1,025 次查看
hiro8235
Contributor I

Hi Kerry.

Thank you for your reply.
OK, I will try to SDK code to the RAM.

Best Regards,

Hiro

0 项奖励
回复

1,022 次查看
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @hiro8235 

  You are welcome!

   If you meet any issues, just let me know.

  If your question is solved, please help to mark the correct answer, just to close this case, any new issues, welcome to create the new question post!

 

Best Regards,

kerry

0 项奖励
回复