Can RT1050 onchip RAM BANK0 be used as NVRAM if I add a Batterry with SNVS power ?
I read datasheet ,I find confilict between Datasheet and AN12085
The datasheet said can't, But appnote said can .
Hi 铁钢 王
seems this is not possible based on Figure 45-1. Power system overview
i.MX RT1050 Reference Manual
https://www.nxp.com/docs/en/reference-manual/IMXRT1050RM.pdf
Could you point where appnote said can.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
What I Think is
Can I simply use a battery that can use the RTC and use RAM BANK0 as NVRAM?
Or I must use NVRAM external ?
Table 8. Description of OCRAM bank
How to use iMXRT Low Power feature, Application Note, Rev. 0, 11/2017
According this table
I think I can use Bank0 as NVRAM, if a battery is added
below this app note, there is no such Table 8
AN12094 Power consumption and measurement of i.MXRT1050