26MHz external crystal for RT600

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

26MHz external crystal for RT600

1,008 Views
mark_wu
Contributor II

Hello,

In i.MX RT600 datasheet show the crystal oscillator operating range 1MHz to 25MHz,

but in the description of clock sources, external clock input pin(50MHz Max),

so can I use a 26MHz external crystal for RT600?

Thanks.

pastedImage_1.png

pastedImage_2.png

Labels (1)
2 Replies

915 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

>> so can I use a 26MHz external crystal for RT600?

No, crystal oscillator operating range 1MHz to 25MHz, SO the customer can not use a 26MHz external crystal for RT600.

External clock input (CLKIN function from a pin, selected by IOCON) is not for the crystal.

Have a nice day.

Best regards

915 Views
mark_wu
Contributor II

Thank you

0 Kudos
Reply