Hello,
In i.MX RT600 datasheet show the crystal oscillator operating range 1MHz to 25MHz,
but in the description of clock sources, external clock input pin(50MHz Max),
so can I use a 26MHz external crystal for RT600?
Thanks.
Hello,
>> so can I use a 26MHz external crystal for RT600?
No, crystal oscillator operating range 1MHz to 25MHz, SO the customer can not use a 26MHz external crystal for RT600.
External clock input (CLKIN function from a pin, selected by IOCON) is not for the crystal.
Have a nice day.
Best regards