Hello, I need your help.
I have MIMXRT1160-EVK witn 1ZM M2 WIFI-BT module.
I was import edgefast_bluetooth/spp example from 2.13 SDK.
Modified define to WIFI_88W8987_BOARD_MURATA_1ZM_M2 in a app_config.h
Build finished it without any errors.
Flashed without any errors.
But it is not working. In a terminal, I see only part of output "[sdio] E"
At pin SDIO_CLK I see 400kHz frequency, about 200ms from board start only.
Help me please with this example.
I’m taking a look into this.
Let me get back to you when I get an update.
Regards,
Daniel.
I checked a few points.
1. Is it ok about 400kHz frequency?
2. I have next oscillograms after power on half second.
SDIO CLK
SDIO CMD
3.
@DanielRuvalcaba Hi, doesn't you have any idea?
Hi @kostya740,
I'm sorry for the late reply.
Could you please tell me if you have removed R183 and added 0ohm resistor at R404 on your board?
Regards,
Daniel.
Hello,
We are still working on your case, we apologize in advance for the time this will take.
As soon as we have some feedback I would let you know.
Hi @kostya740,
Could you please help me with the following information?
Regards,
Daniel.
Hi@DanielRuvalcaba
Thank you for help.
1. Yes. External.
2. I tried. Didn't work too.
3. No. I will do all the need. Thanks.
Do you have another idea? Why didn't BT/WIFI examples work?