1160+1ZM and BT SPP profile

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1160+1ZM and BT SPP profile

1,598 Views
kostya740
Contributor II

Hello, I need your help.

I have MIMXRT1160-EVK witn 1ZM M2 WIFI-BT module.
1.png
I was import edgefast_bluetooth/spp example from 2.13 SDK.
Modified define to WIFI_88W8987_BOARD_MURATA_1ZM_M2 in a app_config.h
2.png
Build finished it without any errors.
3.png
Flashed without any errors.
But it is not working. In a terminal, I see only part of output "[sdio] E"
At pin SDIO_CLK I see 400kHz frequency, about 200ms from board start only.
4.jpg

Help me please with this example.

Tags (4)
0 Kudos
Reply
11 Replies

1,513 Views
kostya740
Contributor II

Hi @DanielRuvalcaba 

It is issue when try wifi_cli example. Could you please help?

image.png

0 Kudos
Reply

1,498 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

I’m taking a look into this.

Let me get back to you when I get an update.

 

Regards,

Daniel.

0 Kudos
Reply

1,478 Views
kostya740
Contributor II

Hi @DanielRuvalcaba 

I checked a few points.

1. Is it ok about 400kHz frequency?
2. I have next oscillograms after power on half second.
SDIO CLK

IMG_5819.jpeg
SDIO CMD

IMG_5818.jpeg

3. 

0 Kudos
Reply

1,409 Views
kostya740
Contributor II

@DanielRuvalcaba Hi, doesn't you have any idea?

0 Kudos
Reply

1,263 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @kostya740,

 

I'm sorry for the late reply.

Could you please tell me if you have removed R183 and added 0ohm resistor at R404 on your board?

 

Regards,

Daniel.

0 Kudos
Reply

1,240 Views
kostya740
Contributor II

Hi,

yes, off course.

0 Kudos
Reply

1,218 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @kostya740,

 

Could you please send me a picture of your whole setup?

 

Regards,

Daniel.

0 Kudos
Reply

872 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @kostya740,

 

By any chance were you able to get the picture of your whole setup?

 

Regards,

Daniel.

0 Kudos
Reply

1,363 Views
nxf77486
NXP TechSupport
NXP TechSupport

Hello,

 

We are still working on your case, we apologize in advance for the time this will take.

As soon as we have some feedback I would let you know.

0 Kudos
Reply

1,576 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi @kostya740,

 

Could you please help me with the following information?

  • Are you using external power?
  • Are you able to run a Wi-Fi example?
  • Did you do the hardware rework as stated in the Hardware Rework Guide for EdgeFast Bluetooth Protocol Abstraction Layer?

Regards,

Daniel.

 

0 Kudos
Reply

1,564 Views
kostya740
Contributor II

Hi@DanielRuvalcaba 

Thank you for help.

1. Yes. External.
2. I tried. Didn't work too.
3. No. I will do all the need. Thanks.

Do you have another idea? Why didn't BT/WIFI examples work?

0 Kudos
Reply