Hello dear NXP team
There is now an API for the 1060 board for the EMMC modules with examples.
Thank you
I am trying to use this example on USDHC2, in 8 bit mode so that we can boot from the part. We are testing the hardware of the board, how do I port the example from USDHC1, we have made some changes but I can see nothing on the logic analyser.
Regards
George
Hi Sergej,
MCUXpresso SDK includes SDMMC drivers and examples in the following path:
SDK_2.7.0_EVK-MIMXRT1060.zip\boards\evkmimxrt1060\sdmmc_examples
You can download it from the following link: Welcome | MCUXpresso SDK Builder
Best regards,
Felipe
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------