有关OpenSDA里面的MK20DX128VFM5芯片固件烧录

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

有关OpenSDA里面的MK20DX128VFM5芯片固件烧录

Jump to solution
5,670 Views
jiangshicong
Contributor III

自己购买的MK20DX128VFM5芯片没有固件,于是自己就去官网上找了一个固件,通过J-link烧录成功后,再去连接电脑,发现电脑还是不能识别OpenSDA,连上电脑没有任何反应,并没有枚举出USB device,怎么解决,有遇到过类似的情况吗????(PS:MK20DX128VFM5芯片是带有熔丝的,我已经报废了三块芯片了,巨坑。。。。。。。)。下面是我下载的固件(感觉这个BootLoader比较正确):

QQ图片20181108193819.png

前两次我下载的固件是(可能固件不对):

QQ图片20181108194515.png

0 Kudos
Reply
1 Solution
4,785 Views
kerryzhou
NXP TechSupport
NXP TechSupport

你找个外部的JLINK, 打开JLINK commander连接你的K20芯片,然后看看是否能找到内核?

如果找不到内核,你输入: unlock kinetis 试试,看看能不能解锁。

如果还是不能不解锁,十有八九被弄锁死了,你需要看下这个文章,看看你哪里有问题:

Kinetis Lock原因的调研及解决方案 


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
4 Replies
4,785 Views
kerryzhou
NXP TechSupport
NXP TechSupport

楼主你好!

K20不会被报废掉,除非你把他们做了最高级别的secure.

另外,你的问题是K20的代码没烧对,你烧了K20的app,所以不能工作,下面你按照我的步骤再来下,就用FRDM-K64的固件吧:

1. 下载K20 bootloader

  https://www.nxp.com/assets/downloads/data/en/snippets-boot-code-headers-monitors/0244_k20dx_bl_0x500... 

下载后,你用外部JLINK 把这个.bin文件给烧到你的K20芯片去。

烧录成功后,板子断电。

2. 烧录app

   这个时候到你Segger页面里面下载对应的FRDM-K64的固件。

SEGGER - The Embedded Experts - Downloads 

   你按住板上reset按键,然后上电,板子应该会模拟出BOOTLOADER磁盘,把你的JLINK固件再丢进这个BOOTLOADER磁盘,重新上电后,你的K20就会成为一个JLINK仿真器。

我不知道你那边用的目标芯片是什么,看你的图片,貌似是I.MXRT,如果不行,还请告诉我你使用的板子和目标芯片型号。


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,785 Views
jiangshicong
Contributor III

你好!我的板子型号是IMXRT1052-EVKB, 我是用J Flash工具去烧录的,烧录一次成功后,第二次想再烧录时,就一直连接不上了,无法烧录。第一次烧录的具体步骤:

step1:按住复位键,点击Target ,然后点击连接,第一次是可以正常连接成功的。

step2:按下键盘F3,擦除芯片

step3:按下键盘F5,烧写芯片

step4:烧写成功,拔掉jlink。重新上电,连接电脑,发现电脑还是无法识别OpenSDA。。

下面是我第二次连接时报的一些错误。

Connecting ...
- Connecting via USB to J-Link device 0
- J-Link firmware: J-Link ARM V8 compiled Nov 28 2014 13:44:46
- Device "MK20DX128XXX5 (ALLOW SECURITY)" selected.
- Target interface speed: 4000 kHz (Fixed)
- VTarget = 3.254V
- InitTarget()
- TotalIRLen = 4, IRPrint = 0x01
- JTAG chain detection found 1 devices:
- #0 Id: 0x4BA00477, IRLen: 04, CoreSight JTAG-DP
- Device will be unsecured now.
- Timeout while unsecuring device. Erase never starts.
- TotalIRLen = 4, IRPrint = 0x01
- JTAG chain detection found 1 devices:
- #0 Id: 0x4BA00477, IRLen: 04, CoreSight JTAG-DP
- Scanning AP map to find all available APs
- AP[2]: Stopped AP scan as end of AP map has been reached
- AP[0]: AHB-AP (IDR: 0x24770011)
- AP[1]: JTAG-AP (IDR: 0x001C0000)
- Iterating through AP map to find AHB-AP to use
- AP[0]: Skipped. Invalid implementer code read from CPUIDVal[31:24] = 0x00
- AP[1]: Skipped. Not an AHB-AP
- Scanning AP map to find all available APs
- AP[2]: Stopped AP scan as end of AP map has been reached
- AP[0]: AHB-AP (IDR: 0x24770011)
- AP[1]: JTAG-AP (IDR: 0x001C0000)
- Iterating through AP map to find AHB-AP to use
- AP[0]: Skipped. Invalid implementer code read from CPUIDVal[31:24] = 0x00
- AP[1]: Skipped. Not an AHB-AP
- InitTarget()
- Device will be unsecured now.
- Timeout while unsecuring device. Erase never starts.
- TotalIRLen = 4, IRPrint = 0x01
- JTAG chain detection found 1 devices:
- #0 Id: 0x4BA00477, IRLen: 04, CoreSight JTAG-DP
- ERROR: Could not find core in Coresight setup
- ERROR: Failed to connect.
Could not establish a connection to target.

微信图片_20181109111713.png

0 Kudos
Reply
4,786 Views
kerryzhou
NXP TechSupport
NXP TechSupport

你找个外部的JLINK, 打开JLINK commander连接你的K20芯片,然后看看是否能找到内核?

如果找不到内核,你输入: unlock kinetis 试试,看看能不能解锁。

如果还是不能不解锁,十有八九被弄锁死了,你需要看下这个文章,看看你哪里有问题:

Kinetis Lock原因的调研及解决方案 


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
4,785 Views
jiangshicong
Contributor III

谢谢。

0 Kudos
Reply