RT1050 CSI OV7670 camera eLCD display

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RT1050 CSI OV7670 camera eLCD display

RT1050 CSI OV7670 camera eLCD display

 

RT1050 CSI OV7670 camera eLCD display

1.Abstract

OV7670 is a CMOS VGA image sensor with small size and low operating voltage. It is controlled by the SCCB bus and can output 8-bit image data of various resolutions with a frame rate of up to 30 frames/second and low cost.

This article mainly implements the use of CSI on RT10XX to obtain OV7670 camera data, and displays it using the eLCDIF display module that comes with RT10XX. The camera and display use RGB565 format. The camera resolution configuration is QVGA 320*240, the LCD is NXP official EVKB matching LCD RK043FN02H, the resolution is 480*272, and the frame rate is 30FPS.

This article is based on NXP official RT1050 SDK:

SDK_2_14_0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\csi\rgb565

Porting the OV7670 driver to implement the CSI method to collect OV7670 image data and display it on the LCD through the eLCDIF module

 

2. Principle explanation

   Here is a brief explanation of relevant knowledge.

2.1 RGB565 Color mode

As a basic color coding format for images, RGB565 refers to a pixel that occupies 2 bytes of data and is usually used in images and display devices. R red, G green, B blue, the actual display can obtain different other colors according to the configuration of the three primary colors. Each pixel bit can display 65536 (2^16) colors. The specific allocation is as follows:

1.jpg

 

Fig 1

From the above figure, we can know that the 2-byte data displayed in pure red, green and blue is:

Red: 0xf800, Green: 0X07E0, Blue: 0X001F

2.2 OV7670 camera hardware and waveform situation

The OV7670 module used is as follows:

2.jpg

Fig 2

Pin situation

No

Signal

Description

1

PWDN

Power consumption selection mode, pull down for normal use

2

RET

Reset port, pull high for normal use

3

D0

Data port output bit 0

4

D1

Data port output bit 1

5

D2

Data port output bit 2

6

D3

Data port output bit 3

7

D4

Data port output bit 4

8

D5

Data port output bit 5

9

D6

Data port output bit 6

10

D7

Data port output bit 7

11

XLK

Clock signal input signal

12

PLK

Pixel clock output signal

13

HS

Horizontal synchronization signal output signal

14

VS

Frame sync clock output signal

15

SDA

SCCB Interface data control

16

SCL

SCCB Interface clock control

17

GND

GND

18

3.3V

3.3V power

RGB565 output data timing:

3.jpg

Fig 3

2.2 CSI frame synchronization signal timing waveform

4.jpg

Fig 4

2.3 LCD display wave

5.jpg

Fig 5

Therefore, the data of OV7670 is obtained through CSI and then stored in the buffer. The eLCDIF then retrieves the data from the buffer and displays it on the LCD screen to display the real-time collection and reality of the camera data.

3 Software and hardware realize

   The test platform is based on NXP MIMXRT1050-EVKB revA1 version:

https://www.nxp.com/design/development-boards/i-mx-evaluation-and-development-boards/i-mx-rt1050-eva...

LCD为:https://www.nxp.com/part/RK043FN02H-CT#/

3.1 Hardware connection

As can be seen from Figure 2, the universal module purchased is a 2.54mm direct plug mode, but the CSI interface used on the MIMXRT1050-EVKB board is an FPC interface, so an adapter board is required to switch from FPC to 2.54mm direct plug mode. The wiring diagram is as follows:   

6.jpg

Fig 6

The actual overall hardware connection situation is as follows:

7.jpg

Fig 7

3.2 Software prepare

Regarding the SDK driver of OV7670, the RT SDK does not provide it directly, but the FRDM-K82 SDK provides relevant drivers that can be transplanted to the RT1050 SDK.   

   SDK version:SDK_2_14_0_EVKB-IMXRT1050\boards\evkbimxrt1050\driver_examples\csi\rgb565

The code replaces the original OV7725 code, replaces the relevant driver with the OV7670 driver, modifies the OV7670 code, matches it to the RT1050 CSI code, and adds IO signal control for OV7670 RST and PWDN. The reason for adding RST and PWDN control is that it was found Some modules, if the RST pin is not closed and delayed to open, will cause the problem of unsuccessful acquisition. However, with the addition of RST and PWDN control, currently OV7670 from different manufacturers can successfully acquire and display stably. For the specific OV7670 code, you can view the attached source code.

The camera initialization code is as follows:  

static void APP_InitCamera(void)
{
    const camera_config_t cameraConfig = {
        .pixelFormat   = kVIDEO_PixelFormatRGB565,
        .bytesPerPixel = APP_BPP,
        .resolution    = FSL_VIDEO_RESOLUTION(320, 240),
        /* Set the camera buffer stride according to panel, so that if
         * camera resoution is smaller than display, it can still be shown
         * correct in the screen.
         */
        .frameBufferLinePitch_Bytes = DEMO_BUFFER_WIDTH * APP_BPP,
        .interface                  = kCAMERA_InterfaceGatedClock,
        .controlFlags               = DEMO_CAMERA_CONTROL_FLAGS,
        .framePerSec                = 30,
    };
    memset(s_frameBuffer, 0, sizeof(s_frameBuffer));
    BOARD_InitCameraResource();
    CAMERA_RECEIVER_Init(&cameraReceiver, &cameraConfig, NULL, NULL);

    if (kStatus_Success != CAMERA_DEVICE_Init(&cameraDevice, &cameraConfig))
    {
        PRINTF("Camera device initialization failed\r\n");
        while (1)
        {
            ;
        }
    }
    CAMERA_DEVICE_Start(&cameraDevice);

    /* Submit the empty frame buffers to buffer queue. */
    for (uint32_t i = 0; i < APP_FRAME_BUFFER_COUNT; i++)
    {
        CAMERA_RECEIVER_SubmitEmptyBuffer(&cameraReceiver, (uint32_t)(s_frameBuffer[i]));
    }
}

The resolution here is QVGA 320*240, which does not match the 480*272 of the LCD, but it does not matter. In fact, the size of 320*240 is displayed in the LCD. If you want to display it to 480*272, you can also configure the size through PXP.

For more code details, see the attached code package.

4. Summary

This article aims to provide a demo of RT OV7670 CSI+eLCDIF acquisition and display. let’s go directly to the finished product effect video. You can see that the relative display is relatively clear, and the refresh effect is also good.

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎11-04-2023 12:54 AM
更新者: