Hello Sirs,
I am using imx8mp ai robot platform, and my code base is imx-yocto-bsp-5.10.72-2.2.3 refers to https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/i-MX-%E6%9C%BA%E5%99%A8%E4%BA%BA%E5%B9%... , howerver when I try to use the rpi-cam-mipi on it,it says it need fw ap1302_ar1355_1080p60_27M.bin,however I cannot found it on the repo https://github.com/ONSemiconductor/ap1302_binaries which is recommended by the rpi-cam-mipi doc, please tell me where to get the corresponding firmware of this camera sensor.
root@imx-robot-foxy:/lib/modules/5.10.72-lts-5.10.y+g26b899af4934/kernel/drivers/staging/media/imx# insmod imx_ap1302.ko
[ 54.541920] imx_ap1302: module is from the staging directory, the quality is unknown, you have been warned.
[ 54.552969] ap1302_mipi 1-003c: ap1302 probe called.
[ 54.558605] Write pca957x error: val=0x1
[ 54.564858] Write pca957x error: val=0x23
[ 54.571489] Write pca957x error: val=0x33
[ 54.577796] Write pca957x error: val=0x37
[ 54.584389] Write pca957x error: val=0x3f
[ 54.588688] Write pca957x error: val=0x1
[ 54.592904] Write pca957x error: val=0xbf
[ 54.630425] ap1302_mipi 1-003c: Direct firmware load for ap1302_ar1355_1080p60_27M.bin failed with error -2
[ 54.640173] ap1302_mipi 1-003c: Falling back to sysfs fallback for: ap1302_ar1355_1080p60_27M.bin
[ 54.649805] ap1302_mipi 1-003c: ap1302_request_firmware failed. ret=-2
[ 54.656384] ap1302_mipi 1-003c: Cannot request ap1302 firmware.
[ 54.664387] ap1302_mipi: probe of 1-003c failed with error -2
Thanks,Sincerely
Solved! Go to Solution.
Sorry for that I forget to share my latest news, I use another bord, it works well!
Thanks!
Finally, I have made the driver works, but I cannot preview the camera or record any YUV data to file, following are details:
[ 2.805324] ap1302_mipi 1-003c: AP1302 Chip ID is 0x265
[ 2.810659] ap1302_mipi 1-003c: Direct firmware load for imx/camera/ap1302.fw failed with error -2
[ 2.813112] ap1302_mipi 1-003c: AP1302 is found
[ 2.819672] ap1302_mipi 1-003c: Falling back to sysfs fallback for: imx/camera/ap1302.fw
[ 6.530390] mx8-img-md: Registered mxc_isi.0.capture as /dev/video3
[ 6.549580] mxc-md 32c00000.bus:camera: Entity type for entity ap1302_mipi 1-003c was not initialized!
[ 6.560558] mx8-img-md: Registered sensor subdevice: ap1302_mipi 1-003c (1)
[ 6.568136] mx8-img-md: created link [mxc_isi.0] => [mxc_isi.0.capture]
[ 6.577608] mx8-img-md: created link [mxc-mipi-csi2.0] => [mxc_isi.0]
[ 6.589038] mx8-img-md: created link [ap1302_mipi 1-003c] => [mxc-mipi-csi2.0]
[ 24.478006] ap1302_mipi 1-003c: Load firmware successfully.
4. use the comand to preview or record YUV data fo file refers to https://docs.nxp.com/bundle/UM11933/page/topics/software_introduction.html , unfortunately it got nothing, no preview on my HDMI monitor, the record file size is 0, here is the terminal log when do preview
root@imx-robot-foxy:~# gst-launch-1.0 -v v4l2src device=/dev/video3 ! "video/x-raw,format=YUY2,width=1280,height=800" ! queue ! waylandsink
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
/GstPipeline:pipelin[ 57.387455] bypass csc
e0/GstV4l2Src:v4l2src0.GstPad:src[ 57.392240] input fmt YUV4
: caps = video/x-raw, format=(str[ 57.397812] output fmt YUYV
ing)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:src: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstQueue:queue0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstCapsFilter:capsfilter0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
/GstPipeline:pipeline0/GstWaylandSink:waylandsink0.GstPad:sink: caps = video/x-raw, format=(string)YUY2, width=(int)1280, height=(int)800, framerate=(fraction)120/1, interlace-mode=(string)progressive, colorimetry=(string)1:4:5:1
[ 1018.967454] audit: type=1006 audit(1651206601.900:4): pid=1459 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
[ 1018.979853] audit: type=1300 audit(1651206601.900:4): arch=c00000b7 syscall=64 success=yes exit=1 a0=3 a1=ffffe9948370 a2=1 a3=ffff90756020 items=0 ppid=416 pid=1459 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="crond" exe="/usr/sbin/crond" key=(null)
[ 1019.005595] audit: type=1327 audit(1651206601.900:4): proctitle=2F7573722F7362696E2F63726F6E64002D6E
^Chandling interrupt.
Interrupt: Stopping pipeline ...
Execution ended after 0:20:14.988214000
Setting pipeline to NULL ...
Freeing pipeline ...
5.I check the voltage test points on RPI-CAM-MIPI board, the voltages are correct.
Please give me some advice to inspect the issue.
Thanks in advance.
do you have imx8mp evk board or 93evk board? I don't have airobot board to test this, but verified on imx8mp evk board, I don't know if this code can work on airobot board or not
Sorry for that I forget to share my latest news, I use another bord, it works well!
Thanks!